Hello guys, I FEEL DESPARATE!!!!!!!
you have a great Community here! :) However, I am a new member so please excuse me for my ignorance.
My problem is LM2576HVT-ADJ... it keeps on dying... actually, I have just burnt the fourth chip... this is getting expensive! But the worse things is, I don't have a clue, why?
The schematics is those found in the Datasheet... a standard one. The load is active, 500 Ohms. The input voltage is 50-60V, provided by AC/DC switching power supply with isolation (a commercial one). The result of the damage is:
-Short from Input to Output
To kill the chip, I have to set the output to something above 30V, while it's working, power-off and then power -on.
The chip starts with little voltage on it, and then (1-2 sec) goes to zero, becoming quite worm is these seconds.
Sometimes this is lucky power-down. But if I let it run for more than several seconds, it shorts output to input hence I have the input voltage at the output.
When this first happened, my flywheel diode was damaged, too. It was a 3A 100V Shottky so I thought I was on the safe side... so I duplicated the diode and the coil (this makes 2 diodes and 2 coils in sequence - supposed to share the current and voltage between them). And it worked - none died afterwards;
In the second death event, the common inductivity was 550 uH (so connected), so I thought I reduced max current to be sound. But again, once I power-down and then power-up, I killed it.
So I added revese diodes (10A, 1000V) on the input and a reverse bypass diode to LM input-output line... just in case something is wrong there. And small ceramic capacitors.
But again, it died at 53-57V...
Finally, I VERY carefully investigated to feeding power supply seeking for current and voltage spikes etc. and surprisingly found NOTHING... moreover, it all looks ideal... okay I said, and added the delayed start to 100 ms or so (with filter to avoid ripples on the input side)... and... JUST FOR A CASE, added TRANSILS TVS 60V on input and 48V on output of the chip.
And just recently when I tried to raise the voltage over 52.5, it died once more. And I still don't understand the reason.
Some more details:
-INPUT Supply: AC/DC 300mA, 5A startup, 50V + - 15V isolated, with short and overcurrent protection and restart...regulated to 50 mv under full load... no spikes and smooth start on and off!
-Input of LM2576HVT-ADJ - 220 uF 100V LowESR capacitor
-Choke values tested - M33 ferrite 1.8A @saturation, 330uH, 550uH, 1080uH
-Diodes: V3J (100V Shottky) 1 or two
-Output capacitor: 1000 uF 100V LowESR
-Load: 10W power resistor R= 500 Ohms
-Strartup delay - 0 to 200 ms tested
-Heatsink: BIG with thermal paste :)
-Regulation of the voltage: R1 (lower) =1284, R2 (upper) = 50k
And, finally, the most interesting thing is, the chips did not get damaged if the inpt voltage raised gradually during operation... it worked well and regulated well! I want to say it once again - to kill it, I have to power-off and the, power on with Vin > 52-57V.
Well.. I FEEL CONFUSED, ... can it happen that all the chips were bad from the beginning?
P.S: I understand that schematics is welcome... but let me do it tomorrow.. tired :(
THANK YOU GUYS FOR ANY HELP OR SUGGESTIONS!
Sergiy.