Hi,
I need to get the output of pin 11 "HG" of LM3150 to be referenced to the ground, not shifted by the switch pin. Some other PWM ICs, it is ok to just connect the "SW" pin to the ground to get this done. But for the LM3150 I found from the internal schematics described in the datasheet, the "SW" pin is having another purposes than level shifting the higher side driver, i.e. it is connected to "ERM control", "Zero Current Detect" etc. I made simulation and found that grounding the "SW" will keep maintaining the regulation function (The high side is shifted back to a proper level by an external circuit).
The simulations do not tell all the story. What is expected when "SW" is grounded? any function, or feature is lost? any other thoughts on this?
Thanks