Hi,
I have a problem with LM3150 IC. During normal operation there is everything ok - I have stable output voltage, and the working freq. is about 250kHz (the input voltage is about 30V and output voltage is 15V).
When I'm making the ESD tests (8kV) to an output of the converter then after the test (discharge) the LM3150 rapidly changes operating freq. to about few hundred Hz, and the IC burn off.
Does anyone knows the reason why the operating freq. decreases so much ? How to secure the circuit against his kind of behaviour ?