Hi,
I am interested in the LM3150.
I have run a simulation for this design specification:
input: 10.8V
output: 0.9V
load: 6A
from the steady state report, it concerns me that the Iin might reach 5.5A peak current.
What will happen if I do not have an input source which is able to supply 5.5A peak current, but rather only able to supply 1A or 2A at 12V-16V?