Hello,
We are using for a low power application (50mA max) the LM46002 converter with the following schematic.
Vout= 5.0V Vin = from 12V to 20V Iout max=50mA
But it doesn't work properly. It raises until 5V then stops and don't restart again until it reaches 3,2V. The switcher just works in the raise ramp then it stops.
Could anyone help?
Thanks in advance.
Bernat Feixas