Looking to us an adjustable Simple Switcher as a current source for a laser diode. The application requires that the laser be blanked and I was curious about how fast the enable on/off pin of the regulator would be able to do this. The application would include a low value current shunt and amplifier to measure the current output and adjust the regulator.
The forward drop of the diode would be somewhere between 3 and 6 volts, forward current being no more than 2 amps.
One requirement of the regulator is that it not have a softstart due to the need for a clean blanking signal.
Any suggestion on a specific regulator and or supporting parts is appreciated.