Could it be possible to generate a Vout=12V using the LM2674M-5.0 changing R1 and R2 in FB (pin4). The idea is to use the same LM2674M-5.0 device to generate Vout=12V or Vout=5V depending of the design
Could it be possible?
thansk in advance
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Could it be possible to generate a Vout=12V using the LM2674M-5.0 changing R1 and R2 in FB (pin4). The idea is to use the same LM2674M-5.0 device to generate Vout=12V or Vout=5V depending of the design
Could it be possible?
thansk in advance
You could possibly hang resistors outside the LM267-5.0 device to change your vout to 12V. But that might not be stable. the internal compensation of the device is tailored for 5V operation. But it might ne alright to prototype the design.
Regards,
Akshay