Hello,
I am using the application note http://www.ti.com/lit/an/snva419c/snva419c.pdf to design a thermal area for the LMZ35003 chip. Reading through the document it appears that θJA is very important and PCB specific. When using equation (10) and calculating board area θJA is subtracted by θJC and 77.5in^2 is divided by that result. Because the 77.5 and θJC are constants (θJC is package dependent) it seems like a higher θJA will reduce board size. But I would think you would want to reduce θJA so that your thermal resistance is low and therefore dissipated more heat easily?
It seems like using θCA would be a better calculation to use because it would give me the thermal resistance of the actual board i design. However θCA is not used in any of the calculations, can i substitute it for θJA? It would be great to talk to an FAE on the phone if possible to help clear this up and go through the example i currently have.
Thanks,
Brandon