I'd like to use the LM2586 to make a 300 V supply at about 10-15 mA, with a 24 V input.
I've built it and it seems to work well.
I have some questions though:
1) Size is critical, and the webbench circuit calls out 100 uF output cap (350 V) which it going to be a problem.
I built it with the 22 uF cap I had on hand and it seems ok using the 47uF/1.78K values suggested by webbench.
Will there be a stability problem if I use a small output cap?
I haven't seen any information on design of the compensation network and its relation to the output cap size.
Thanks