Hi,
Am trying to design a circuit powered from an 1.5V cell, i have chosen the TPS61220 to boost the 1.5V to 3V and am having some issues
first , applying recommended value of 4.7uH inductor made a huge output voltage drop, i tested some value , the only usable value for me is 100uH inductor and 470uF capacitor , otherwise i get terrible output wave form.
second with those values of L and output C, i get an efficiency between 30% to 50%
i tested with some pure resistive load and this is what i get
load 1K
Input current 12.5mA
Input voltage 1.5V
Output current 3mA
Output voltage 3V
Eff around 50%
load 250R
Input current 66mA
Outout current 12mA
Eff around 36%
The load i need the powerup with the TPS61220 is a BLE module most the time on sleep mode ( 300µA ) with pic current about 40mA when active.
I can't understand what am doing wrong, so any help please.