Hello,
I tried to bring up AN-2027 on this subject and the message said that it was either removed or the name has changed. I am using the LMZ14203/LMZ14203H in a power supply design and I would like to also use it for my -V needs in this design for part commonality. I would like to know if I can do this with a Non-Isolated module and if so what I need to be aware of to make this work reliably. My input V is from a battery Min. +21.5V, Max. +28V. Output -20VDC ~500mA.
Thank You,
Jeff