I am using an LMR62014 to generate 20V at 100 mA. The output briefly goes to 25V and then thermal shutdown quickly kicks in. If I lower the load resistance the output goes to 30V and then I again get thermal shutdown. The voltage on the feedback pin is around 1.2V, but there is a lot of noise on it. The load is purely resistive. I am using the schematic from the datasheet and a layout very close to that as well. The inductor is 10 uH, the feedback resistors are 200K and 13.3K, and the feedback capacitor is 130 pF. Any thoughts on what I might be doing wrong.