I am using the Texas Instruments LM2594M-ADJ in a new product design. Do you know what the maximum reverse voltage is from the OUTPUT pin to the +Vin pin? I basically just need to know if a protection diode should be placed between OUTPUT and +Vin to prevent the reverse voltage from getting too high when the input voltage goes to 0 on power-down and there is still 5V being held up by the output cap. The circuit is set up for 5V output.
I've seen this done with other linear regulators in the past but not sure if it is really needed.
Thanks,
Mark