Hi. I am testing an adjustable constant current source circuit as described in attached file. I am testing it now with LMZ21700. I know that LMZ21700 works in DAC adjusted Vout, but does it also work in DAC adjusted Iout circuit?. Are there any concerns or requirements when using the circuit?. In case LMZ21700 doesn't work, can you suggest any ICs that can work with the circuit?. My system requirement as following.
1. Inductor integrated DC/DC converter.
2. DAC's Slew rate 1.2V/us. DAC Full Scale =2.5V.
3. Time to settled Vout = 2ms(Max)
4. Load resistance = 30 to 40 Ohms
5. Iout range = 60 to 120 mA.