Hi Team,
Our customer would like to know the light load efficiency of LMR14030.
However, we can’t confirm this value on Webench.
Could you please let us know if you have any data?
They would like to evaluate the following conditions.
And, they expect the efficiency 85% at Iout=10mA to 20mA.
If the efficiency is less than 85%, could you please let us know if you have any recommended device?
[Conditions]
-Vin=32V to 32V
-Vout=12V
-Iout=3.0A(max)
-Light load output current=10mA to 20mA
Regards,
Kanemaru