Dear All,
I need more than the 5amps which gives the IC LM2678. I would like to as if i could put some of them for example 4 in parallel to increase the output current.
Is that possible?
Thank you in advance for your time.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Mr. Anston
the specs are :
Input 24 volt
Output 1: 12volt 10 - 12 amps
Output 2: 13.8 volt - 10 amps as SLA battery charger.
So could you propose me some other IC which could achieve those specs?
Thanks\ for your time.
Dear Mr. Lobo,
The Ic you propose to me it does not have output of 12 or 13,8volts. Only 6. I could not use it.
Thank you for your time.