Hello E2E forum!
I am looking for additional information on the LM46002 which I am not able to find.
1. I know from experience that the feedback path with the resistor divider can cause problems, especially if a technician decides to probe that net...the output will take a big step (not good). What I am looking for there is some scheme for output over-voltage protection. I plan to use smaller value resistors to help minimize the issue with technician probing on the board. But, if there is a short from the feedback pin to the common, then the input voltage might show up at the output.
2. What happens if the LM46002 fails? I mean, if it were to fail will it fail open or short?
My biggest concern with any DC-DC converter is protection of loads at the output. If there are simple things I can do to prevent this event, it seems prudent to do so.
Any feedback or input is welcomed and appreciated!
Thanks again!
Paul