Is it a limit bandwith of signal that I can put to LMZ21700's Feedback pin?. I want to connect Opamp Output as feedback to the pin, so ultimately I want to know the GBW of Opamp that fits. I see that the switching frequency of LMZ21700 is around 1.8~2 MHz at Vin=5V, does it mean I have to pick the Op Amp's GBW around that value?