Hello, I am designing a board where I use LMR14006 (or LMR16006). The input voltage is 12 or 24V.
The board needs approx 100-200mA maximum load but the board will "sleep" for most of the time and I need a low current consumption (1-2mA).
Using webench I get an error if I use LMR140006 at low current (I used 5mA) which is a bit surprising as I understand that this device is supposed to work at light load.
With LMR16006 it works in webench at 5mA.
Is there a difference between them at light load ? Should I use the 16006 ?
Thank you,
Mihai