Hello,
I am new to power regulation and working on a project where minimizing power consumption is imperative (fairly low noise would be good too). Can I receive assistance in estimating the power consumption of the LM3150 (Vin=8.2 V and Vout=3.3 V, and I believe the current draw for the load is probably ~1 A or so max)?. Also, are there any suggestions in minimizing the power consumption with this component and/or suggestions for a better one? Thank you and I appreciate your time and consideration!
Regards,
Nate