Is there any limit on the O/P Capacitor for LMZ14203HTZ ?
My Specs are Vin = 24 V , Vout = 15V , from 0.2 Amp to 2 Amps .
I intend to use 10 Nos of 22uF / 25 V Ceramic MLCC ,1206 Size ; Ceff = 220 uF
Thanks and regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there any limit on the O/P Capacitor for LMZ14203HTZ ?
My Specs are Vin = 24 V , Vout = 15V , from 0.2 Amp to 2 Amps .
I intend to use 10 Nos of 22uF / 25 V Ceramic MLCC ,1206 Size ; Ceff = 220 uF
Thanks and regards
Hello Denislav
Thanks for your prompt reply .
Yes, we are using 22 nF as Feed Forward Capacitor .
One more Q pl : Is there any lower limit on the ESR of the O/P Capacitor ?
Second , does the LMZ14203HT require a minimum value of O/P Ripple for Control stability ?
Thanks and Rgds
Hello Varunesh,
Good question. The COT architecture needs some ESR ripple from the output capacitor for stability.
However the LMZ14203H uses a control scheme which derives most of the necessary ripple from the low side power FET Rdson. This allows you to use low ESR capacitors (i.e. ceramics) on the output. On the other end, too much ESR (along with the feed forward capacitor passing through all the ripple to FB) can trip the OVP protection. Section 8.2 of the datasheet has a schematic with component values (Figure 46). There is a suggested ESR range for the output capacitor (assuming Cff is 0.022uF).
Cheers,
Denislav