I am using the LMR70503 for a negative supply. In the datasheet it calls out a 6.8uH coil in the Application Circuit Bill of Materials. I looked at the datasheet for this coil and the current and resistance ratings that are mentioned in the LMR70503 datasheet do not match the ratings for the VLS2012ET-6R8M datasheet. I just wanted to point this out. The ratings in the coil's datasheet are lower current and higher resistance (.64A typical and .415 Ohms typical). Is this still ok for the LMR70503 application? Please clarify this.
Thank you,
Michael Nycz