Hello everyone,
I have an application where I would like to use the LMZ14201 to track another voltage. The 'special features' section of its product page states 'tracking'. But the datasheet does not mention how to achieve tracking. Could anyone provide some details please?
Specifically, I would like the LMZ14201 to track an external voltage, but be 2.7V higher than the external voltage. The tracking circuit will also need to limit the output voltage of the LMZ14201 to 6V (the maximum allowed output voltage). The external voltage is a charging capacitor, which can take values from 0V up to 4.2V.
Thank you for any help,
Ben