Hi,
I am using a LMZ22005 Simple Switcher for generating 3.3V power supply, and I need some clarification about its minimum input working voltage. I found some contradiction in the datasheet :
- The LMZ22005 datasheet says that its input voltage range is [6V ; 20V] on page 1
- But on page 3 it says that it is [7V ; 20V] for 3.3V output voltage
- But in the same time, on page 6, there is a figure that shows 3.3V operation with 6V input voltage (fig. 8)
Is the minimum input voltage 6V or is it 7V for 3.3V operation ? What happens is this is 7V and its actual input voltage is 6V ? This is really important for me as I will be using a 2 cell Li-Ion battery with a voltage that can be as low as 6V.
I also have a similar problem with the LMZ12001. I need to generate a voltage of at least 3.7V with an input voltage that can go as low as 6V. What is the LMZ12001 minimum input voltage for 3.7V operation ?
Thank you for your help,
Regards,
Maxime Puech