Hi My customer is looking for,
I’m looking at a suitable boost converter to use with bq51025 Wireless Power Receiver Evaluation Module. This is to boost the voltage from 10V to 13.5V.
From LMR61428 Evaluation Module datasheet, it seems only do up to 5V /500mA.
From LMR62014, as it is, it can produce 12V / 450mA.
Can either of the EVMs be modified to give 13.5V / 1A outout?
Sujeeva Wettasinghe
Avnet FAE