In my application, VIN is 15V, Vout will be 5V. I am not planning on using the enable input. The enable input is rated to 5.5V max. There is internal 20M pull-up to VIN on enable. Question is, is it ok to float the enable line with Vin 15V. Or I need external voltage divider?