Hello,
I'm wondering if the LM2576 gets damaged if a voltage higher than the set output voltage is applied to the output of the switcher? What is the allowed maximum voltage on the output of the switcher?
Thank you very much in advance.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm wondering if the LM2576 gets damaged if a voltage higher than the set output voltage is applied to the output of the switcher? What is the allowed maximum voltage on the output of the switcher?
Thank you very much in advance.
Hello,
The output voltage is controlled by the feedback divider. Do you have an alternate way to power the load? Please send us your schematic. The problem arises when the voltage at the output goes higher than the input voltage. This can damage the device. The max voltage at the output is limited by the max duty cycle and the input voltage.
Regards,
Akshay
Hi Kally,
When the output is short to a higher voltage than the input of the LM2576, the body diode of the internal MOSFET will turn on to conduct current from OUTPUT to VIN. That might damage the LM2576. The solution is to add a schottky diode from the OUTPUT pin to the VIN pin to redirect the current through the schottky, to protect the LM2576. You can also add a zener diode at the output to clamp the voltage. The zener voltage should be higher than Vout, say 16V zener with Vout = 12. Then the output voltage wouldn't be higher than the input voltage.
-Yang