Hi,
I am using both the LMZ14202 and the LMZ12002 Simple Switchers to output 12V and 3V respectively. I'm currently powering the board using a wall adapter but I will eventually be powering from a 16.8V battery pack. The 3V regulator is powered from the 12V regulated output.
I have calculated RFBT and RFBB using the datasheet equations and double checked my results using TI's online calculator (WEBENCH). I'm a bit confused however since the equations in the datasheet do not take the input voltage into account and suggest resistors be chosen between 1 and 10k. But the WEBENCH suggests larger resistors whose values change with a change in input voltage.
What I'm seeing is that as I change the wall adapter output the 12V regulated output changes as does the 3V regulated output. When I check the voltages on an oscilloscope however the voltages are steady (no noticeable ripple). My concern is that once I'm powering from a battery, since the battery's output will fluctuate, so will all of my voltage rails. The switchers are supposed to maintain a stead voltage are they not?? (within reason, input voltage varying by 1.5V). I'm using the suggested capacitor value and voltage ratings, what else can I do to ensure a steady voltage? How come the datasheet calculations are different from WEBENCH?
Thanks in advance for any suggestions!