I have a question about how could we protect the LM2735 and its components L1 / D1 from a short circuit on the load side.
The circuit used is the typical one :
Vin = 5V
Vout = 12V,100mA
At the beginning I use a CTP (LITTELFUSE 2016L030DR) for that purpose at the output side, but this cause a voltage drop due to the CTP itself.
So, to avoid this voltage drop, could I put the fuse in the input side ? Is this solution efficient ? Any drawback ?
All advice would be welcome.
Thanks.
:-)