This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Behavior of LMR14050 at Ta=80℃

Other Parts Discussed in Thread: LMR14050

Hello

I simulated LMR14050 under Vin=3 ~ 36V, Vout=5V, Iout=4.2A, Ta=-30℃, 80℃.
But when Ta is 80℃, this device couldn't simulate.
Can it behave above the condition?
Please let me know recommending operating range of the Ta.


Best regards,


Yokota