Hello everyone.
I am currently working in GPRS based sollution and i am planning to use an LM2596.
These are the parameters:
Vin: 40V
Vout: 5V
The measured current of the circuit is 700mA (with GPRS transmitting and receiving)
I know the GPRS module have 2A burst. Should I choose the external components with that burst in mind or should I choose them according my current needs?
Which other regulator would you reccomend for this design?
Thanks,
Javier.