I have been looking at some of the LM258x line of dc-dc boost converters. I need to output 24-30V (anywhere in that range) at 0.5A from an input of 7.4-8.4V (2S li-ion battery), and I want a through-hole regulator (TO-220 package) which has a minimum of external components.
While searching through the datasheet for the LM2588 for a schematic for a boost circuit I found this line: "For applications with different output voltages, refer to the Switchers Made Simple™software" (p 23, top). I cannot find this software. Is there a newer version of this software which would let me make a custom design with the LM258x?
Thank you for your advice.