We are using the LM2674MX-5.0 in a circuit that has a max load current of about 100-150mA.
This circuit part of a product that is used in conjunction with a medical linear accelerator that produces high energy (6MV) X-ray radiation.
The product/part never exposed to a direct radiation beam, it is subject to scatter component of the beam only.
We have found that the output of this fixed 5.0 volt regulator drops to about 4.6 volts over a period of about 1.5-2.0 years and needs to be replaced.
The part continues to regulate at the reduced voltage even under load... but is obviously well out of tolerance.
We are suspecting radiation exposure as the root cause... and are weighing our options for designing the component out of the circuit.
Have any other engineers experienced this type of "slow-n-soft" radiation induced component failure with the LM2674MX-5.0? (or other switching regulator)
In addition, do any engineers have knowledge of a fixed 5.0 Volt regulator that has good radiation tolerance?
It is my assumption that an internally adjusted (laser trimmed) reference voltage/current source within the part is getting altered (re-trimmed) by radiation exposure... however, the surrounding regulation/feedback circuitry just keeps regulating accordingly.
Kevin D.