Hi,
Using the LMR14030 for a buck converter,the expected output power is 10W(5V/2A),
How to calculate the minimum input voltage for this application?would you please provide
a formular for me?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Using the LMR14030 for a buck converter,the expected output power is 10W(5V/2A),
How to calculate the minimum input voltage for this application?would you please provide
a formular for me?
Thanks!
Moving to the Simple Switcher forum...but you can get the information you need by looking at the drop out curves of Figures 7, 8 and 9 of the datasheet.
John,
Thanks! But there are no dropout curves in the datasheet for some parts,please tell me how to calculate it for this case.
Hi Jerry,
The dropout voltage varies with many facts. Such as frequency, inductance, inductor Rds_on, inductor resistance. You can use below equation for an estimated calculation:
Vin=Vo+Io*(Rds_on+RL)+(1-Dmax)*(Vd+Io*RL+Vo)/Dmax
Rds_on: High side FET on resistance
RL: indictor resistance
Vd: diode forward voltage
Dmax=1-Toff_min/(6*Ts) for frequency lower than 1MHz, Dmax=1-Toff_min/(11*Ts) for frequency higher than 1MHz.
Toff is 120ns typically. Ts is period of a switching cycle.
BR
Luke
Hi Jerry,
Toff_min may become larger when switching period (Ts) increases. but it's not as large as Ts in proportion. That's why Dmax varies with frequency.
BR
Luke