In the LMR62014 data sheet can be read:
SHUTDOWN PIN OPERATION
The device is turned off by pulling the shutdown pin low. If this function is not going to be used, the pin should be
tied directly to VIN. If the SHDN function will be needed, a pull-up resistor must be used to VIN (approximately
50k-100kΩ recommended). The SHDN pin must not be left unterminated.
I want to control the shutdown pin using a uC but I want it to be down when the uC is at deep sleep mode (controlling GPIO in high impedance).
Is it possible to use a pull down resistor at SHDN pin?
If there is a pull up resistor inside the chip in this pin, which is the value of that resistor?
Thank you in advance.