I want to use some Simple Switcher modules (LMZ31530, LMZ31505) to provide various power supplies for a Kintex FPGA. I need to make sure that they are sequenced correctly. Looking at the parts enable and power good pins it seems as though I can just connect the power good from the first parts in the sequence to the enable pins of the next parts in the sequence. There is a Kintex reference design that uses these parts but it uses a controller to do the sequencing.
Thanks