Sir, I used LM2576adj for my circuit,Actually this circuit for automotive applications,thats why i want to some protective circuit also ,please suggest me what type of circuit i have to use...? INPUTS- 6-24v
outputs 3.9v, 2amp
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Sir, I used LM2576adj for my circuit,Actually this circuit for automotive applications,thats why i want to some protective circuit also ,please suggest me what type of circuit i have to use...? INPUTS- 6-24v
outputs 3.9v, 2amp
Hi,
Was there more to this question before it was moved to this forum? I am not clear what you are requesting.
Regards,
MArc
Hai,sorry for the inconvenience.Actually,i am using 'IL2576adj',for SMPS for the automotive purpose ,but the thing is the voltage range is increasing in some conditions ,so i would like to have some protection circuit for SMPS .The input to the SMPS is 5-20 V,but sometimes,when the vehicle gets started it gradually increases upto 40V. The output of SMPS is 3.9V ,2Amp.So that i need some circuit for the protection.Kindly help me out of this problem.