Want to control the Enable Pin of the LM46000 over external logic. During power-down the Enable voltage could be higher then the Input Voltage. It seemed, that there is a Diode between Enable-Pin and Input-Pin.
How high must be the Enable-resistor between logic and LM46000 (or what is the maximum current of the protection diode of the LM46000)?
thanks and best regards
Bertram