Hi!
our application is class D amplifier.
We want to use lm5576 as our negative power source and follow TI webench reference design. please find the attached file.
DC In : DC-12V
DC out: DC-N50V
when power up, DC-12V buck to DC-N50V, it work fine without load.
But when add 50ohm load, it only buck to N30V and the switch pin (pin17.18) not stable.
Could someone help us to check the reference design is correct?
We can't find the formula and information between COMP(pin6) and FB(pin5) in the negative mode from datasheet.
kuda
https://webench.ti.com/webench5/power/webench5.cgi?origin=ti_panel&lang_chosen=en_US&VinMin=45&VinMax=45&O1V=-48&O1I=0.5&op_TA=30