We are using two LMZ31506 6A SIMPLE SWITCHER® Power Modules that operate with 12VDC In and 5.5VDC at 4.2Amp Out and 5.6VDC at 4.5Amp Out. We are operating at 800 KHz switching frequency. These supply's are driving a synthesizer and RF circuits. We see the 800KHz switching spurs on the RF signal from the synthesizer. I did an experiment using power supply signals wired from a second board to a first board with the power supplies removed. The spurious signals when away. This leads me to believe that I have ground currents from the power supply's getting into the synthesizer. I want to isolate the power ground from the synthesizer and RF circuits ground. How should the power supply outputs be connected? Should filters be used for the ground connection?