Using the LM2676S-ADJEVM board (and 2 circuit boards that I've designed), there is a certain condition that can cause a significant overshoot in the output voltage. This is caused by the startup circuit inside of the part, and can go higher than 7.7V in a 5V system. It occurs if the input power is interrupted for a short time, allowing the output to drop below 5V before the input power is re-applied. The LM22676 does not seem to have this problem. An easy way to see the problem is to diode-couple a variable supply into the output to keep the output slightly below 5V when the input power is removed. When the input power is re-applied, the output will overshoot to higher levels while the startup circuit activates. There is a burst of switching cycles before the feedback circuit detects the output over-voltage condition. The overshoot is also dependent on the input voltage. The EVM on my desk is showing an overshoot peak at 7.72V when 17.3V is applied to the input while the output is at 4.9V. This problem does not show in my WebBench simulations. We had many field failures (over several years) until I finally observed this window of failure conditions. More information can be provided if needed.
good luck!
Carl