Hi,
I am using LMZ31707 for generating 3.3V from 12V. I would like 3.3V to start after another supply of 5V is stable. The Switcher which generates 5V does not have PGOOD signal. Hence in order to sequence 3.3V after 5V has reached say 4.5V, can I connect the UVLO circuit through R1/R2 to 5V of LMZ31707. The PVIN and VIN in this case is 12V. Table-11 in LMZ datasheet provides resistor values for RUVLO1 = 68.1K and RUVLO2 = 24.3
It is mentioned in Fig 40 and 41 of datasheet that UVLO Resistor divider is always connected to VIN or PVIN or both but there is no mention of a supply other than VIN/PVIN. Please let me know if this is fine.
Regards,
Shareef