What is the equation used to determine the power dissipation of the LMZ36002?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is the equation used to determine the power dissipation of the LMZ36002?
With input voltage, output voltage, output current, and switching frequency... how would you determine Iin or Power Dissipation? The above equation assumes you know the total part's power dissipation or input current, which would be a factory of losses and switching frequency.
The power dissipation curves in the datasheet are only for the recommended switching frequency. Operating at another switching frequency will effect the power dissipation. An EVM can be used to measure power dissipation for other operating conditions.
Thank you for the response... I appreciate the options to use the datasheet, simulate on Webrench, and/or use a development module... but I'm looking for a way to calculate these items given the known inputs. Typically TI includes a Power Dissipation equation within their datasheet to Calculate the theoretical value. I view this as an analytical means to calculate power dissipation instead of an empirical or simulation mechanism... that's ultimately what I'm looking for in this situation is the analytical means for calculating power dissipation when knowing the variables of input voltage, output voltage, output load, and frequency.
Thanks,
Ryan