For a Master-Project from my University we have to power three actors in a 3D stereo lithographic printer.
We would like to use the IC LM22676MRE-5.0/NOPB with an Input of Vin: 12V and we need Vout: 5V/4,5A.
In the Datasheet they say the CL Current Limit is Min: 3.3A and Max: 5.5A. Is it possible to get 4,5A with the normal configuration?
Or do we need a special configuration? Many thaks in advance!
Benjamin Mattmüller