Hi,
Can you please provide the following information for the TPS3828-33DBVT part?
1. Junction Temperature Max (Tj Max)
2. Thermal Resistance Junction to Ambient (Theta JA)
Thanks in Advance
Dibin Mathew
Hi Dibin,
The TPS3828 is a low power supervisor with IDD typically 15uA and 400uA (max) current through the open drain RESET output. Because the power is so low, the junction temperature will practically be the ambient temperture. Therefore, the max Tj is +85 deg C.
Regards,
Darwin
Hi Darwin,
Can u plz give the thermal resistance value-junction to ambient for this IC.
Thanks and regards
For this older datsheet, it is found under the dissipation rating table on page 4 as operating factor. Theta JA would be the the inverse of 3.5mW / degC.
1) The inverse of 3.5mW/C is 286C/W.
2) From the DISSIPATION RATINGS table of the data sheet, the maximum dissipation at 85C is 227mW.
3) Therefore to address the original question, the maximum allowable junction temperature of this device would have to be 150C correct?
(227mW * 286C/W + 85C) = 150C
Hi Kurt,
That's correct.