In a new design, I’m using a TPS3808 to supervise the voltage of an AA battery. If the voltage is below 0.9 V then the RST pin switches to another battery. In another circuit of the same project, the RST pin simply turns off a switching regulator and allows current from another power supply to supply the circuits powered by the converter just turned off. I selected the version 0.9 because AAs don’t have much more juice left below 0.9 V. In re-reading the datasheet I was not sure about the specs. In page 2 it shows TPS3808G09 with a nominal supply voltage of 0.9 V and a threshold voltage of 0.84 V. What is 0.9 V? Should I use the version G01 and add two resistors so I can have a thresold a bit highr that 0.84? Or should I live it with the 0.9 V version? Why is the threshold voltage so low in the G01 version (0.405 V)? The supervisory chips are powered by a 3 V power supply powered by a lithium battery which cannot be turned off.