From the block diagram of the SLUS247f.pdf, I dont see the relation of the watchdog with the nRES output.. The only connection that connects the two are the Q output of the SR flipflop to the NAND gate.. If I look at the timing diagram of figure 4, the reset output is somehow related to the transition of the WDI and output of the WDO.. HOw is this possible if the block digram doesnt show any feedback to the reset function..
Is figure 4 possible if I do the next paragraph after that figure 4?.. CONNECTING WDO TO RES?.. Please advise as I am definitely lost in this document..