Hi,
We are working on a project where we use Delay Supervisor TPS3808G09DBVR for voltage monitoring. We used dot matrix board and tested the circuit with Ct of 270pF which should give a reset delay of 2.04ms. When it is tested for different iterations, we found that the reset delay not being consistent and varying to 20ms. Is this because of testing locally on Dot Matrix Board? Will the reset delay be consistent if PCB is used? Have somebody experienced the same? Please help to resolve the issue.