Hi members
This is BEN.
My customer consider the TPS3820-33.
Please supporting
Q1: In the case of WDI-pin is open, the voltage of WDI-pin happens to?
(Internal circuit of WDI-pin What are the?)
Q2: I understand that push-pull is RESET-pin.
Do you have an internal resistance of each Hi-side/Low-side?
In some cases, Error range and resistance value how much?
Q3: In the case of RESET is to output Hi,
It has no problem even if the Low from the IC another external?
Best regard
BEN.