Dear, All
Is it satisfactory even if it thinks that the ESD diode is not attached to "MR pin" of TPS3808G01-Q1?
Thanks, Masami M.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear, All
Is it satisfactory even if it thinks that the ESD diode is not attached to "MR pin" of TPS3808G01-Q1?
Thanks, Masami M.
Hi, Ryan
Again, it indicates.
Is the ESD diode built in "MR pin" of TPS3808G01-Q1?
Thanks, Masami M.
Hi, Ryan
"MR pin" of TPS3808G01-Q1 is indicated to be "-0.3V to 7V" by absolute-maximum-rating regulation.
Is it right although I think that the diode for ESD protection will not be contained between "MR pin" and Vdd from now on?
Thanks, Masami M.
Hi Masami,
Sorry about the misunderstanding. You are correct, there is no ESD diode between /MR and Vdd that would prevent /MR from being tied higher than Vdd so long as you remain within the absolute maximum conditions.
Very Respectfully,
Ryan